Posts From June 2024

TDK’s immunity software now supports testing per AIM 7351731

Jun 27 2024 in News  

Testing per AIM 7351731 [Medical Electrical Equipment and System Electromagnetic Immunity Test for Exposure to Radio Frequency Identification (RFID) Readers] is now supported in TDK Radiated Immunity Lab and TDK Conducted Immunity Lab software. AIM 7351731 is a standard that provides specialized guidance on the testing of non-implantable medical devices to determine if they are immune...
Read More >

Visit us at IEEE EMC+SIPI 2024 in Phoenix, Arizona, USA, August 5-9, 2024

Jun 21 2024   

TDK will be an exhibitor at the 2024 IEEE EMC+SIPI International Symposium on Electromagnetic Compatibility, Signal & Power Integrity in Phoenix, Arizona, USA, August 5-9, 2024. Come visit our booth at the Phoenix Convention Center.


Read More >

PAGE TOP