Jul 31 2026 in News
TDK will be an exhibitor and paper presenter at the 2026 IEEE EMC+SIPI International Symposium on Electromagnetic Compatibility, Signal & Power Integrity in Dallas, Texas, USA, August 3-7, 2026.
Mar 31 2026 in News
Testing per AIM 7351731 [Medical Electrical Equipment and System Electromagnetic Immunity Test for Exposure to Radio Frequency Identification (RFID) Readers] is now supported in TDK Radiated Immunity Lab and TDK Conducted Immunity Lab software. AIM 7351731 is a standard that provides specialized guidance on the testing of non-implantable medical devices to determine if they are immune...
Read More >
Apr 15 2024 in News
TDK RF Solutions is the winner of the Silver IGUS Vector Award for 2024. This winning project involved positioning numerous antenna assemblies for interference resistance tests.
Jan 20 2023 in News
TDK offers a wide range of radio wave absorbing materials based on our long tradition of developing electrical and magnetic material technologies as well as electronic and radio wave technologies.
The latest lineup of TDK RF absorber materials is presented in the updated "Radio Wave Absorbers" catalog. We are excited to introduce IP-030C, a shorter EMC absorber solution, and IS-V,...
Read More >
Jan 18 2023 in News
If you intend to use a hybrid antenna for final compliance measurements as per ANSI C63.4-2014, then the antenna must meet the symmetry requirements called out in Annex N of the document. But which condition should be used to determine compliance? Condition A or Condition B? And what frequency range is required for the symmetry test?
TDK has made available online an article...
Read More >
Jan 12 2023 in News
The TDK EFG-03 is a unique E-field generator designed to produce controlled, high intensity electric fields over the frequency range of 10 kHz to 100 MHz. The EFG-03's integrated mast provides complete manual control of height, tilt, and polarization. The EFG-03 provides the e-field you need for your testing.
Jan 04 2021 in News
TDK is excited to announce the new
HLP-2008A Hybrid Log Periodic Antenna. The HLP-2008A is an extended frequency broadband antenna intended for measurements in an anechoic chamber, open area test site, or in situ. Its 20 MHz to 8 GHz range makes it the widest emission antenna in its class. It is especially suited for wideband testing of radiated emissions from electrical and...
Read More >
Jun 25 2020 in News
TDK announces that TDK TestLab, a suite of software packages to handle EMC testing, EUT monitoring and antenna measurements, now includes support for testing integrated circuits according to the following standards:
IEC 61967-2: Integrated circuits - Measurement of electromagnetic emissions, 150 kHz to 1 GHz - Part 2: Measurement of radiated emissions - TEM cell and wideband TEM...May 29 2020 in News
TDK announces the release of its new EMC chamber lighting solution, the HBLED-540 High Bay LED Light Fixture.
With its minimal RF emissions, this new luminaire is ideal for lighting EMC chambers.
The prismatic borosilicate of the HBLED-540's glass sustains maximum levels of luminosity over time and does not fade, discolor or diminish.
The High Bay LED...
Read More >
Apr 24 2020 in News
TDK RF Solutions introduces its new lightweight tripod model
TRI-350R tripod. This sturdy, lightweight, portable, non-conductive tripod is designed specifically for mounting antennas, video cameras and other instruments in EMC test environments. The tripod is constructed of light but strong fiberglass and plastic to provide the necessary stability. The tripod legs fold inward and...
Read More >