Mar 31 2026 in News
Testing per AIM 7351731 [Medical Electrical Equipment and System Electromagnetic Immunity Test for Exposure to Radio Frequency Identification (RFID) Readers] is now supported in TDK Radiated Immunity Lab and TDK Conducted Immunity Lab software. AIM 7351731 is a standard that provides specialized guidance on the testing of non-implantable medical devices to determine if they are immune to emissions from radio frequency identification (RFID) systems. TDK's radiated immunity and conducted immunity software packages support testing to AIM 7351731.
The standard provides medical device manufacturers and end-users with guidance on how to evaluate their devices for immunity to emissions from RFID systems. The test procedures in this document are based on experimental results from several AIM members. Test protocols are included for the major commercial implementations of RFID as standardized by ISO, including LF, HF, and UHF RFID. Both active and passive ISO RFID standards are covered in this document.